Currently, the Delta DVP Series can read/write network data with other devices through the ETHRW command. Please refer to the
DVP Operation Manual - Programming for detailed instructions. Note that if you use the DVP-SE/ES2-E, EH3 built-in Ethernet communication port, the communication port number (S
1+2) is K108. For others, such as DVP-SA2/SS2/SX2 and so on, please use the DVPEN01 communication module on the left side of the host to execute ETHRW commands. Its communication port numbers are K100~K107. K100 is the communication module adjacent to the host, while K107 is the most distant.