What's the biggest difference between the old PR mode of the ASDA-AB and the new PR mode of the ASDA-A2?
Please refer to the comparison table below.
The Ways to Call a PR
There are 64 position settings in PR mode. PR 0 is homing mode and the others (PR 1 ~ 63) can be user-defined. For the ways to call a PR, please refer to the table below: