What is PUU provided in ASDA-A2 series?The PUU (Pulse of User Unit) is a unit which is scaled by the electronic gear. This will bring out an advantage, and that is “YOU SEE WHAT YOU COMMAND”. For example, if you send 10000 PUU for command and you can read from the feedback 10000 PUU by ignoring the E-Gear Ratio and vise versa.
Please refer to the figure below for more explanation.