Description: If the “00-20 Master Frequency Command Source” is 9, the “08-65 PID Target Value Source” setting will automatically change to 1. Users then cannot set the 00-20 to other control authorities.
A: Adjust the 08-65 to 0, and set the 00-20 based on users’ needs.