Method 1:
Run ASDA-Soft and select the Parameter Editor. Input 10 for the parameter P2-08, and press “Enter” to cycle the power.
Method 2:
Please refer to the operation manual for the panel parameter setting. Set the parameter P2-08 as 10 and cycle the power.