What is the meaning of the symbol marked after parameter code? What should the user pay attention to it?The explanation of symbols marked after parameter codes are shown as the following. Please pay close attention to it before setting these parameters.
(★) Read-only register, such as P0-00, P0-01, P4-00.
(▲) Parameter cannot be set when Servo On (when the servo drive is enabled).
(●) Parameter is effective only after the servo drive is restarted (after switching power off and on), such as P1-01.
(■) Parameter setting values are not retained when power is off.