- Fill in an absolute path in Directory to Scan (e.g., D:\).
- Enter the CSV file name in File Spec.
- Leave empty CMEP MEPMD01 Standard.
- Select Header Row in File as the template file has a header.
- Select File Use Unique Keys as the MachineID in the template file lists equipment IDs. As this is row A, which stands for row zero counting from zero, enter “0” in Key Column (0-based).
- Leave empty Parameters in One Column.
- Keep the default setting in File Time Zone.
- Directory Scan Rate (secs) stands for the rate of scanning for the CSV file.
- File Process Rate (secs) stands for the rate of processing for the CSV file.
- Trigger stands for the conditions triggering the function.