How do I change the logic of the I/O terminal signals for the Delta Vector Control Drive C2000 Series?
The I/O terminal signals refer to the digital input and output signals. The logic of the input signals can be changed with the 02-12 parameter setting, and the output signals with the 02-18 setting. See the illustration below.