When a motion control card’s pulse interface receives input, the Compare Trigger function facilitates real-time value matching enabled by the FPGA of the card. Differential signals are output when values are matched. The user can create interval diagrams with computer software to set signal output positions, which allows the control of camera shooting. Illustration as follows.