FAQ
What is the password to log into the software DRAS to operate the Robot Controller with the Servo Drive Integrated ASDA-MS Series?If you wish to modify advanced settings when using DRAS, a password is needed to login (see image 1).
The default password is noted on the side label on the control (see image 2).
Please use the last 8 characters of the MAC to log in (see image 3).

Have a question? We'd love to hear from you. Inquiry