How does regenerative resistor affect the servo drive?A regenerative resistor is used to discharge the regenerative power returned from the motor to the servo drive which is generated when the servo motor runs and stops a load with a large amount of inertia frequently. This regenerative power is transmitted into the capacitance of DC bus, resulting in the rise of voltage. When the voltage rises to a certain high level, the servo drive will need to dissipate the extra energy by using a regenerative resistor. In general, when the capacity of the regenerative power is small, there is no need to install a regenerative resistor. Use the regenerative resistor when:
1.A regeneration error (ALE05) is detected on the servo drive during the operation.
2.The DC bus voltage exceeds 370V or the output torque of the servo motor exceeds 100% constantly.