There are three kinds of gantry motion with different coupling strengths between two axes.
1. Position control with two axes: weak coupling
2. Position control with the main axis, and speed control with the secondary axis: medium coupling
3. Position control with the main axis, and torque control with the secondary axis: strong coupling
Example 1: A one-piece linear module or carriage for the Y-axis;
Example 2: Two motors drive a screw, i.e., the two axes drive a single device.
Gantry motion settings:
1. Use the parameter P1-01 Control Mode to configure the tracking mode for the secondary axis.
2. Use the parameter P2-58 to enable the gantry function and commands.

3. Use the following parameters to adjust tracking of the secondary axis.
P2-54 -> The Gain of Synchronous Speed Control
P2-55 -> Integral Compensation to Synchronous Speed
P2-56 -> Integral Compensation to Synchronous Position
P2-57 -> The Bandwidth of Synchronous Control