How do I set up parameters to connect the Compact Drive MS300 with the digital keypad KPC-CC01?The communication protocol for the Compact Drive MS300 is ASCII 9600, 7, N, 2 by default.
For the digital keypad KPC-CC01, it is RTU 19200, 8, N, 2 by default.
Please set the parameters as follows to connect the MS300 with the KPC-CC01.
Pr.09.00 = 1, 09.01 = 19.2, 09.04 = 13