There are two types of projects for DXMC: DMARS (system configuration files) and KW (PLC program).‧ DMARS (system configuration files) Click the button “On-line Operate” to set up the connection between the DXMC and your computer (as shown in the screenshot below). When the DXMC and your computer is connected, it automatically checks an imported system configuration file. If the file is inconsistent with the default file or the previous file saved in DXMC, it will download automatically to the DXMC.

‧ KW (PLC program) Please download a project manually. Click “Project Control Dialog” > “More”. Then tick “Permanent as boot project” and click “Download”.