The flow chart of Fig. 1 shows the process.1. Refer to page 17 in the DMV3000 User Manual (Fig. 2).2. Define a camera FOV range.3. Select a camera and a lens.4. Find an online lens calculator to calculate the optical resolution. If the resolution does not meet your requirements, go back to Step 3 and reselect a camera and lens.Fig. 1: Flow Chart

Fig. 2: Page 17 in the DMV3000G User Manual