Please refer to the following application parameter groups. Currently the supported industrial applications are for compressor (IM), fan, pump, and air handling unit. We also provide a user-defined parameter setting function.

For example, if you select the industry parameter “2”, the built-in compressor parameters will be set.