Is there any version of Delta’s PLC programming software WPLSoft or ISPSoft compatible with the Linux system?Currently, both WPLSoft and ISPSoft can only be operated on Windows, and neither is compatible with Linux. The only way to use WPLSoft, ISPSoft, or other Delta Industrial Automation software on any operating systems other than Windows (e.g. Mac, Linux) is to install a virtual machine software and run the Windows OS in parallel. Also, we suggest you install ISPSoft instead of WPLSoft since ISPSoft is the new programming software with more functions.