If a synchronous error occurs between two ASDA-A2 series servo drives, the user must correct the error through a host (external) controller. However, if a synchronous error occurs while using the ASDA-M series, the data of the two axes is exchanged in the same CPU without any time delay and the error is corrected immediately, providing excellent real time synchronous control. The host (external) controller is almost eliminated.