The brake signal controls the solenoid valve, provides power to the brake, and enables the brake. Please refer to the operation below to set the DO functions and wiring.
1. Digital output (DO) setting: Set the DO code to 0x08 (BRKR). When the signal of electromagnetic brake control is output, refer to the setting of parameters P1-42 and P1-43.

2. Refer to the wiring diagram below to use an electromagnetic brake.

Notes: (1) The brake coil has no polarity.(2) Do not use brake power and control power (VDD) at the same time.