How do I use the input terminals VS+ and VS- of the Power Supply Module AH Series?
Make sure that the input terminals VS+ and VS- of the Power Supply Module AH Series connect to an external 24V power supply, then please use the special data register SR731 to examine if the voltage input is stable.
If the 24V input is unsteady, please use the 24V Low Voltage Detection Interrupt task, I34, to trigger the logical control.