Use the built-in function “Linear Transformation” in the Equipment Variables of I/O Communication.

(We recommend you use the Linear Transformation function instead of dividing the value by 10 in time script.)
As the screen shot shows above, we use the Linear Transformation function to transform the captured data into calculable data. For example: If 1000 is the captured value of PLC D:300/WORD, then the value is displayed as 100 in D300.
While using this function, please note:
1. The Min. and Max. values have to match the actual captured values.
2. The associated variable Var.EXT1.D300 must be within the range of calculable values.