Click “coord” in OFFSET group. Five setting options are available:
1.AUTO: Automatically insert the current position of the axes to the selected coordinate system (G54~G59)
2.ABS: Manually insert the absolute coordinate values of the systems
3.INC: Manually insert the incremental coordinate values of the systems
4.SQUARE: Guides the user in setting up the coordinate value of the object center with the diagram. Set the values of the four points, and convert them to calculate the value of the object center. (Please refer to the picture below)

5.CIRCLE: Suitable for setting up the values of the circular object center. Select any three points in contact with the circular object, and set up the three points’ values at the same time to automatically calculate the coordinate value of the object center. (Please refer to the picture below)