The camera of the Delta Machine Vision System DMV2000 Series is equipped with two standard COM ports CH1 & CH2. Which port is for general purpose use?
The camera is equipped with two standard COM ports CH1 & CH2 (Picture 1.) For general purpose use, please plug the Camera Link cable on the CH1 port to connect with the Camera-1 port on the DMV2000 Series.