Please explain the maximum working range and payload of the current Delta Articulated Robot DRV Series models.
The Delta Articulated Robot DRV Series offers four models with a maximum working range from 70cm to 1.4m. The maximum payload is 7kg for all models. Please refer to the detailed specifications below: