The sockets of the AS300 series PLC transmit and receive the user-defined communication codes. It usually communicates with a non-Modbus TCP device via Ethernet.
Please refer to the steps below to set up and enable the sockets:
1. Enter HWCONFIG, double click the Host icon, and select Ethernet Port Advanced Setting→Socket Function Enable.

2. Set up the communication protocol: TCP or UDP.

3. After setting, use the instruction codes below to enable the sockets in the editor.