You can check if the distance between the center of gravity and the 6th axis’ vertical / horizontal flange is within the limited range based on the payload curve graphic. Each product series has different payload curves and limits, so you can refer to our official website and determine which robot is suitable for your needs.
(The following graphic shows the range of payloads and center of gravity for the DRV70L/ 90L Series.)