1. Set up the Basic DI/DO Relay Multifunction Power Meter DPM-C501L Series’ station number to station 4, Baud Rate to 9600bps, and parity bit to 8n1.
2. Set up connection of the IEEE 802.11 a/b/g/n Wireless AP DVW Series under the condition when the IP of the DPM-C501L and the setup computer are in the same domain name.
3. Connect the DVW Series to the DPM-C501L with the DVW Series’ serial port 1, and check if the connection succeeds via the Modbus cache.
4. Disable the IGMP and the AMPDU functions in the DVW Series to set up a wireless network.
5. Input IP Address and Station number to connect the DVW Series to the programming software DPMsoft, as shown below. For IP Address, input the DVW Series’ IP information and the DPM-C501L’s IP for Station. Press the “Connect” button after input.

6. The interface of the DPMsoft will display a green indication banner when connected.