1. When wiring, connect the inverters’ DC+/DC- terminals to the REG Series’ DC+/DC- terminals, as shown in the wiring diagram below.
2. If drivers are connected to reactors, the reactors should be installed at the position of the DC Choke as shown in the wiring diagram.
3. The wiring distance between the EMI filter and the Power Regenerative Unit must not exceed 10 meters, and the power supply for these components should not provide power for other devices.
4. Remove the ground short circuit from the Power Regenerative Unit.
5. If the Power Regenerative Unit is not equipped with an EMI filter, please install an induction-based (no capacitance) EMI filter to avoid damaged capacitors caused by harmonics. If your equipment is equipped with a phase order protector, we suggest installing an OEM EMI filter.