Yes. Without changing any settings, the CNC controllers connect the linear scale to motor drives, forming a double closed loop control and sending feedback signals. The linear scale feedback function eliminates errors from connecting screw and motor drives and enhances processing precision without affecting the motor’s original feedback function. (For more information on the motor drive’s closed loop control, please refer to the ASDA-A2 manual.)