What are the differences between the C200 series and C2000 series AC motor drives?The AC motor drive C200 series is designed for light-duty load applications up to 10HP and replaces the VFD-B series. It fits the requirements of the low-power inverter market. The C2000 series is designed for normal-duty to heavy-duty load applications.