1. Select "C InPt" and change the input mode of the counter to batch counting

2. Select input (Up, Down, Up/Down ABC) and output (F,N,C,R) mode

3. Connects trigger with the CP1 to start counting: When the count number is equal to the set unit of the batch number (e.g. 10 units / batch), the OUT1 will output value 1 to the batch number, while the count number will reset to zero for next round counting. When the batch number is equal to the total set batch (e.g. 20 batches), OUT 2 will output signal which means the current batch counting is completed. (The RST1 and RST2 can reset the count number and batch number to zero).