The results of the Shape function built in the Machine Vision System DMV2000 Series can be transmitted to register 1010H-104FH via RS-232 communication protocol. Users can then set up the MODICON drive with the SCADA system to output results to the system. In addition, the DMV2000 Series can trigger cameras to take photos via register 1000H.