How could the AC motor drive output voltage measured by a user be as high as 600V?The voltage the user has measured is the DC voltage at PWM output. The user actually needs to measure the AC motor drive output voltage using an electric meter with RMS function or an analog meter.