Why would the output current of an AC motor drive measured with a handheld multi-meter show a different value than the inverter?The handheld multi-meter can precisely measure the AC motor drive’s current in the range of 40 ~ 60Hz. If the current does not fall within this range (40 ~ 60Hz) the measured value may deviate.