What are the advantages of installing a transducer at the drive’s input side?.To lower the AC motor drive’s harmonics.
.To lower the surrounding voltage and current impact on the AC motor drive, such as the surge voltage, the current of surrounding devices, and the surge voltage of the mains.
.To improve the power factor.