Is SCADA System DIAView identical to e-Server?It is feasible to add variable tags in DIAView for data monitoring. After setting the tags as history variables, it is possible to use specific time interval records (one record per second at minimum) or variation records to save the tag information into SQL server compact. The built-in template allows users to import history variables into reports based on the predefined formulae, and automatically create history reports to assigned files.