Is the CameraLink wiring of Delta’s Machine Vision System DMV2000 directional?Yes, it is directional. CameraLink has predefined specific pins with different bandwidths for data transfer. The wiring marked “Camera Side” for users offers proper connections that optimize the transmission speed. Even if the wiring is not properly connected, the bandwidth used for CameraLink can still function, but with lower transmission efficiency. Longer wirings may have more electrical resistance, which may cause inefficient transmission or image transmission failure.