A Tag Table is a list of tag names to replace the use of addresses. A Tag Table defines what the address is so it can be easily chosen for use. Open Tag Table from Options> to start editing a new label by adding a new tag.

After adding the new tag, give the tag a name. The name should be easy to remember and without special characters other than English letters and numbers. Choose the type of address for the read address, either BIT or WORD, the address for this tag, and lastly enter the description for this tag name. If necessary, the Tag Table may be exported to an excel sheet for easier insertion of new tag names to be imported back later. To use these tag names when inputting a read/write address, choose the tag list and the tag name.