How do I start or end the operation of a Delta SCARA robot? There are three ways to start, suspend (halt) or stop SCARA robot operation:
1. Match the Digital Input (DI) circuit on the robot controller with push buttons on operating machines.
2. Adopt the Delta Robotic Integration Software (DROE) user interface.
3. Set parameter commands for precise coordination of operation via the MODBUS communication protocol.