For the C2000 series AC motor drive, how do you use the built-in PLC function to record the frequency at power failure?The frequency at power failure can be recorded by setting M1005 (fault indication for the C2000) and special D1020 (output frequency) with delay time, such as shown in the figure: