The built-in PLC function of the C2000 can execute the process control. The C2000’s built-in PLC function can write up to 10K steps.

D0: 1st step operation frequency
D1: 1st step speed acceleration time
D2: 1st step speed deceleration time
D3: 1st step continuous duration
D4: 2nd step operation frequency
D5: 2nd step speed acceleration time
D6: 2nd step speed deceleration time
D7: 2nd step continuous duration
After trigger M0, the process curve runs as: