Usually, there are two modes. For the open-loop mode, the speed is calculated by the equation: n=120f/P to estimate motor speed.

For the close-loop mode, an encoder is mounted to the motor. The encoder feedback (signal) is sent to the PG card for displaying the actual motor speed. In this case, the motor speed is precisely controlled.