For the latest release of the SCADA System DIAView 3.1.0.0 version for IO communication with Delta power meters, you can select DPM-C530 Ethernet as the driver option for easy IP setup and port connection. Another choice is via DPM-C530 Serial with a setup that includes simple baud rate setting, digital bits, marking, and verification method.

Examples of Setup:
1) Ethernet setup - IP: 192.168.1.5; Port: 502
2) Serial setup - Baud rate: 9600; Digital bits: 8 bits; Marking: 1; Verification method: None