When completing the setup and identification of linear motors from the A2R manual, high frequency noise often occurs due to an increase of motor current control. To resolve this problem, please adjust the parameter value PM-15 (current loop proportional gain) to half of its original setup value, which will reduce the high frequency noise.