What would happen if a 3-phase model of the C2000 series AC motor drive encountered phase loss under single phase power conditions? Would the drive continue to operate?The 3-phase C2000 drive would continue to operate under single phase power for light duty applications. For heavy duty applications, the 3-phase C2000 drive would emit an alarm and stop the drive according to the method set in parameter Pr.06-53 Treatment to the Input Phase Loss.