Delta’s HMI editing software DOPSoft provides convenient communication with other host equipment or software such as SCADA. Users can store the data in the register via TCP/IP, RS-232 or RS-485 communication and easily read the statistics and related data of the HMI on the DIAView SCADA System.
HMI connection status

DIAView connection status