Is there any restriction on ambient and operation temperatures when using an AC motor drive?
Yes, the temperature protection level is stated in the user manual and the operation temperature range may vary among the different AC motor drive series. Please refer to the user manual for more detailed information. Below is an example from C2000 series, showing the Operation Temperature and Protection Level, and the Derating Curve if the ambient temperature is higher than the restricted range.