Yes. First, connect the platinum RTD to the C2000 drive as shown in the following diagram. Then set the C2000 drive to output a steady current of 9mA at the AFM2 terminal and detect the voltage on the AVI terminal. Since the resistance of PT100 would change according to the temperature, the user can then find the current temperature by detecting the AVI voltage.

To set up the C2000 AC motor drive:
1.Set Pr.03-23 = 23 and Pr.03-33 = 45 to output a steady 9mA current at the AFM2 terminal.
2.Set Pr.03-00 = 11, use AVI to detect the voltage on PT100.
3.Check the PT100 temperature chart to find the corresponding resistance value and calculate the voltage according to the value:
.Resistance * Steady Current = Voltage
.When temperature =135°C, the resistance will be 151.71ohms. The voltage can then be calculated by 151.71*9mA = 1.37V.
.When temperature =150°C, the resistance will be 157.33ohms. The voltage can then be calculated by 157.33*9mA= 1.42V.
4.If the user wants to lower the frequency to 10Hz as the temperature reaches 135°C, set Pr.06-56 = 1.37 and Pr.06-58 = 10
5.If the user wants the drive to output a warning and stop operation at 150°C, set Pr.06-57=1.42 and Pr.06-29=1.