For a C2000 series AC motor drive, how do you properly connect PG pulse input terminals A2,/A2,B2,/B2 for the open collector (OC) input function?Please refer to the following diagram for wiring information.
(If you wish to increase the resistor capacity, the suggested range is 1k~2k Ohm, 1/2w.)