How do peripheral devices used in robotic solutions communicate with Delta SCARA robots? Delta SCARA robots support serial communications including RS-232, RS-485 and Ethernet, and communication protocols such as MODBUS and MODBUS/TCP. Peripheral devices can communicate with Delta SCARA robots if they support the same serial communications and protocols.